Industry Online Support
Technical Forum
8/25/2011 3:52 PM | |
Posts: 495 Rating: (58) |
Hi franciscomosse, you can´t use the ESC and the OK key in the LOGO! program! Only the function keys and the arrow keys are usable. Regards |
8/25/2011 3:52 PM | |
Posts: 2930 Rating: (432)
|
Hi, to controll a function in the programm the ESC and Enter can not be used. But to use the Arrow keys ESC must be pressed additional. Regards |
8/26/2011 2:45 PM | |
Posts: 495 Rating: (58) |
Hello, follow this LINK>>... In this threat you can find a post from Betel which includes a download with examples for menu control. Maybe it helps |
8/26/2011 3:17 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (714) |
There is another menu example on the Logo example page: https://www.automation.siemens.com/mcms/programmable-logic-controller/en/logic-module-logo/application-examples/Pages/Default.aspx Have a look there too. Regards, Marcjan |
Problem solved? |
|
Follow us on