Industry Online Support
Technical Forum
9/27/2011 7:04 PM | |
Posts: 63 Rating: (1) |
I want to print all the alarm that happened with clicking on the button? can i also save this alarm on an exel file? |
9/28/2011 7:46 AM | |
Joined: 9/8/2005 Last visit: 9/11/2024 Posts: 177 Rating: (15) |
Hello, unfortunately, only from WinCC version 6.2 you can activate in the Alarm control a button to export the displayed alarms in a CSV file. For Excel it is quit easy to open such a CSV file. If you want to export the alarms automatically in the background or with an button click earlier, you can use the WinCC Add-on PM-OPEN EXPORT:www.siemens.com\pm-open-export Michel |
Last edited by: Michel at: 9/28/2011 7:48 AM |
|
Follow us on