9/29/2011 7:38 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, Pick a TOF with a time off 3sec. TW= input for duration KT= n.i n= time value 0---999 i = multiplier 0= 0.01s,1=0.1s,2=1s, 3=10s R= reset, 200 does not have that DU = actual time dual coded DE = actualtime BCD coded Q = output You can read the actual time of a 200 timer as integer. See attachment for TOF help. Regards, Marcjan AttachmentPrinting _Off-Delay Timer.pdf (111 Downloads) |
Problem solved? |
|
9/29/2011 6:29 PM | |
Posts: 24 Rating: (0) |
I'll try it !! Thanks. Fernando |
Follow us on