Industry Online Support
Technical Forum
10/4/2011 4:49 PM | |
Posts: 2 Rating: (0) |
I've got the source, just dont know if its the newest... so i would like uploading the component, to be sure.. |
10/6/2011 3:55 PM | |
Posts: 3037 Rating: (192)
|
Hello,
This is not possible because WinCCflexible does notsupport such a compare function.
Its possible to load up a backup from Panel with Prosave, butyou can not edit this backup (just restore to apanel wich are the same type). Else it is possible to upload a project (source), but for this you have to activate this option at the download of the project.Take a look at this FAQ: How do you back transfer the projects of an operator panel and what should you watch out for? Best regards |
Follow us on