10/4/2011 10:12 AM | |
Posts: 150 Rating: (5) |
dear all, i have problem with line choke connected with a 611 u system. The configuration is attached. in the system the choke is getting heated up although we have checked the current and voltage are balanced and in range. Choke type no. 6SL3000-0DE21-6AA0 please help. Also Can we introduce breaking resistance in the system if yes can any one give some type no. or neccassary info regarding the same. regards simatic manager AttachmentPresent system.pdf (274 Downloads) |
Follow us on