Industry Online Support
Technical Forum
12/1/2011 10:06 PM | |
Joined: 8/16/2010 Last visit: 5/16/2024 Posts: 636 Rating: (12) |
Hi all. I have question about starting and stoping 3 motors. Motor M1 can be started if motor M2 OR motor M3 was started. When stoping motors, if M1 not working, M2 or M3 immediately stop when press stop taster. If M1 working and press stop of M2 or M3 immediately stop M1 and after 5s stop M2 or M3. M2 and M3 blocikng each other. how to realize stopping of motors? AttachmentLAD.pdf (53 Downloads) |
12/2/2011 2:58 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (714)
|
Hello, Something like in attachment. I used Set and Reset instructions, makes it easy to program the conditions to start/ stop the motors. Regards, Marcjan AttachmentFC6.pdf (56 Downloads) |
Problem solved? |
|
Follow us on