12/6/2011 8:49 AM | |
Posts: 165 Rating:
|
Hi to all The SIMOTION C Controllers are generally supplied with the current firmware version. The C230-2 firmware is installed on the device and the MMC Card for this controller is delivered without firmware. The C240/C240 PN does not contain any firmware, it directly uses the firmware installed on the MMC-Card. If you wish to use another firmware version this can be achieved by replacing the firmware on the MMC Card of either controller. " AttachmentMMC_error_during_erase.zip (441 Downloads) |
Follow us on