12/27/2011 9:48 AM | |
Posts: 5 Rating: (0) |
can we communicate S7-300 & S5 to WINCC with the same CP card |
12/27/2011 9:59 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
What is the type of CP? best regards, Hristo Mihalev |
12/27/2011 10:19 AM | |
Posts: 5 Rating: (0) |
CP5611 and CP1430 |
12/27/2011 10:21 AM | |
Posts: 5 Rating: (0) |
communication of S5-135U and S7-300 form WINCC 7.0 with the same CP card is that posible ? |
12/28/2011 5:50 AM | |
Posts: 5 Rating: (0) |
if we use CP 5611 for the communication of S5-135U & S7-300 to WINCC so is it communicate or not |
Follow us on