Industry Online Support
Technical Forum
1/6/2012 12:27 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, If you have two ET200S PN CPUs, you can just create an S7 connection in Netpro between them, and use the functions PUT and GET or USEND/URCV in one or both CPUs (The S7 connection works in both directions, there is not really a Master/slave in that case). Here an example how to use PUT and GET: http://support.automation.siemens.com/WW/view/en/18610307 The ET200S CPUs work just like S7-300 CPUs of the mentionned example. |
Last edited by: jklm at: 1/6/2012 12:30 PMBest regards |
|
Follow us on