3/1/2012 4:51 PM | |
Posts: 32 Rating: (1) |
Dear All ... Can i use ISI ASCII MODULE with part no 6ES7 138-4DF01-OABO with IM 151 - 3PN system... With Kind Regards Pradeep Prabhu B |
3/2/2012 8:10 AM | |
Joined: 10/7/2005 Last visit: 4/28/2024 Posts: 3004 Rating: (1046)
|
Hello PRADEEP PRABHU B I'd say you can, the 6ES7138-4DF01-0AB0certainly exists inside the Hardware cataloge of anIM151-3can be configured as part ofit, so you should be right. |
Cheers |
|
3/2/2012 5:30 PM | |
Posts: 32 Rating: (1) |
Dear Sir... Thanks For Replying.. I just confuced after refering mannual as attached.. In page no 12... it has mantioned that it will not support.. With Kind Regards Pradeep Prabhu B Attachmentet200s_im151_3_pn_manual_en-US_en-US.pdf (59 Downloads) |
3/3/2012 1:10 AM | |
Joined: 10/7/2005 Last visit: 4/28/2024 Posts: 3004 Rating: (1046)
|
Hello PRADEEP PRABHU B I fear there is a typing mistake in the manual. The 1SI module is available in the followingtwo versions (see also HERE for more): 1.) 6ES7138-4DF01-0AB0: ASCII/3964R (old version:-4DF00) 2.) 6ES7138-4DF11-0AB0: Modbus/USS(old version: -4DF10) For some strange reasons the manual you mentioned, lists the 4DF01 as type "Modbus/USS"which is wrong. Having said that, it also states that the 4DF01 is only not supported up to product release 4, the current4DF01is however product release 5 (see HERE) and hencesupported in the IM151-3 (and it is also available for selection underneath the various IM151-3's in the Step 7 HWcatalogue). My advise is as such as before, you will befine using it, but it won't hurt if you seek clarification via a Support Request from Siemens and please up posted about the outcome. I hope this helps |
Cheers |
|
Follow us on