Industry Online Support
Technical Forum
3/23/2012 11:29 AM | |
Joined: 10/3/2008 Last visit: 5/22/2024 Posts: 957 Rating: (123) |
Hi, yes, it's possible. The modbus block for S7 1200 is integrated in V11. If you want to use CP343-1 or CP443-1 you need the OpenModbusTCP blocks. It's not possible to install the software in V11, because it's for V5.4 and V5.5. But you can copy the modbus blocks into a new project and migrate the project to V11. Then you can use the modbus blocks for CP343-1 and CP443-1 in V11. It works. Wüstenräuber |
Last edited by: Wuestenraeuber at: 3/23/2012 11:33 AM |
|
3/24/2012 4:03 AM | |
Posts: 50 Rating: (1) |
Wow, that's funny. Thanks you so much, Wuestenraeuber |
Follow us on