Industry Online Support
Technical Forum
3/27/2012 3:20 PM | |
Posts: 3037 Rating:
|
You should stop the archiving with the function "StopLogging" and then you should use the function "CloseAllLogs".
You can create a button with these functions CloseAllLogs,ArchiveLogFile, and OpenAllLogsunder the event click. The functions wait for each other until the previous function is ended.
There are no difference whether you use an event on a button or you use an event of the scheduler. How are tags and alarms logged in WinCC flexible? How do you do long-term archiving with WinCC flexible? Tweety |
This contribution was helpful to
1 thankful Users |
Follow us on