4/1/2009 10:38 AM | |
Posts: 22 Rating: (0) |
Post the file in the forum, maybe you have to edit manualy to try correct it comparing to others files. |
4/1/2009 11:46 AM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
How can I edit manually the file? |
4/1/2009 11:52 AM | |
Joined: 5/28/2008 Last visit: 4/26/2024 Posts: 1343 Rating: (141) |
I think he means to attach it as zip-file in a post. Then we can have a look about it. |
3/28/2012 8:08 PM | |
Posts: 46 Rating: (8) |
I have the same problem. The processor is password protected so I cannot upload. The password from my machine builder is supposed to be 1010 but it does not work. The backup file from my supplier is corrupt. It will not open with MicroWIN V4.0 SP9. The backup which gets created does not open either. I have attached the orginal file. If you find a way to open it please let me know. I get this message: ------------------------------------------------------------------------------------------------------------------------------------------------ System Error: Comparing data for internal decisions. An internal error has occured. Although a backup copy of this project will be saved, it may contain inconsistent data. ------------------------------------------------------------------------------------------------------------------------------------------------ Then I get this message as Micro/WIN exits: ======================================================================== Micro/WIN Executable has stopped working. A problem caused the program to stop working correctly. Windows will close the program and notify you if a solution is available. ======================================================================== AttachmentSBCL for forum.zip (118 Downloads) |
Follow us on