4/12/2012 9:01 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, To start with the cable http://support.automation.siemens.com/WW/view/en/27609308 That is a USB cable, there is allso a RS232 one, but Real RS232 ports are not on every laptop anymore. The new Logo 0BA7 you can program by ethernet. You don't really need a memory card, that'smore used for easy programming more than 1 logo with same program or to protect your program against copying, depends on type off card. Battery card you need if the backup time off the Logo itself is to short( 80H). The program will always stay in the Logo, only retentive data will be lost and you need to set the clock after long power down. Regards, Marcjan |
Last edited by: Marcjan at: 4/12/2012 9:04 AMProblem solved? |
|
4/12/2012 9:08 AM | |
Posts: 22 Rating: (1) |
Huh? What do you mean by USB programming? you taking of Rs232? |
4/12/2012 10:23 AM | |
Posts: 8 Rating: (0) |
Hello, I think i know enough to get started. Tank you all for helping. Kind regards, Rick
|
This contribution was helpful to1 thankful Users |
Follow us on