Industry Online Support
Technical Forum
5/4/2012 11:47 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166) |
Hello, Please have a look at the following link: Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? and: Which organization blocks do you need for error handling? Best regards, Wizard |
5/4/2012 7:15 PM | |
Joined: 4/30/2007 Last visit: 3/9/2023 Posts: 231 Rating: (23) |
Hello Martin, take a look also in this link Diagnostic package PNIODiag for diagnostic evaluation for PROFIBUS DP and PROFINET IO |
Follow us on