Industry Online Support
Technical Forum
5/6/2012 7:12 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello Ammy/Darius, i think something is mixed up here for me I think Per Olof is asking to retain internal Tag value. But is it possible? Well, it is cleasr that DB Can retain the Value. But for Per Olof question i don't think it is possible. So Better to Create new Share DB inside PLC logic for your requirement. |
VANDE MATARAM..... |
|
5/6/2012 10:52 PM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating:
|
Hello Amit_86, I think Something is not undestand you correctly, Per_Olof Say Hello all, Thanks for all answers! Yes it is an internal tag. An I run the application on a PC runtime. Okay I will use a receipe to store the data. Which DB is retained in teh PLC for ET200s ? Thanks all! now DB you have already mention about how to do it, & me also. also have a look on this post. ET200s, Retain valuesI think People need rest on Weekend..... |
Ammy |
|
This contribution was helpful to
1 thankful Users |
Follow us on