Industry Online Support
Technical Forum
5/4/2012 11:01 PM | |
Posts: 153 Rating: (15) |
Hi.all. I loaded into a module the program via a Wi-Fi. It is my first experience with the 7th series. I Can forbid IP changes such as with the password. |
5/6/2012 12:14 PM | |
Posts: 40 Rating: (1) |
Can you please show how it is done |
5/7/2012 8:14 AM | |
Posts: 2930 Rating: (432)
|
Hi, if you configure the WLAN Router right, then it is no problem to connect to LOGO! 0BA7 via WLAN. Regards |
This contribution was helpful to1 thankful Users |
5/7/2012 11:25 AM | |
Posts: 153 Rating: (15) |
Hi,Helmut13. You are rigth. The problem was in a router. Hi,Mohamed Asharaf. Network structure in the attached file. |
5/7/2012 12:06 PM | |
Posts: 153 Rating: (15) |
Hi, Existence of port ethernet gives advantages at work with this 7 series. It's fine. |
Follow us on