5/7/2012 5:08 PM | |
Joined: 2/8/2007 Last visit: 8/2/2024 Posts: 12 Rating:
|
hello, I calculate the optimal cycle time with this formula: CT = ((T75-T0) - 1.25*(T75-T25))/10 CT = Cycle Time T75 = Time at 75% of change of PV T25 = Time at 25% of change of PV T0 = Time at 0% of change of PV the rules that use are: put the control in manual (example: output = 15%) wait for the stabilization increase of 10% (example: output = 25%). save T0 wait for the stabilization T25 and T75 calculated as the time to reach 25% and 75% of change I use also this formula form my on-line Tune |
This contribution was helpful to
2 thankful Users |
5/8/2012 9:04 AM | |
Joined: 2/8/2007 Last visit: 8/2/2024 Posts: 12 Rating:
|
i share, in my site, a implementation of FB41 with a sample time programmable and a parameters switch.... link to download: http://blog.ranghetto.com/?p=167 i use a "timer" maked withsystem tick (sfc64) also i make a cascade controller look inside my library ;) |
Follow us on