5/18/2012 10:43 AM | |
Joined: 10/9/2007 Last visit: 8/1/2024 Posts: 1248 Rating: (115) |
Hi Umencho Yes,I meant manuals. There is only some information here www.sicam.de This is an internal decision and there aresome reasons to do it. Themost part ofpeople who need more detailed information about Sicam has contact with Energy Automation sector, so they can get extra information. Others could be potential customers - and this is whyI suggest these to contact Siemens - or competitors. My participation on this forum started because of WinCC (base for Sicam HMI) and S7. But then I noticed that some colleagues asked for solutions for energy automation, DNP3or IEC61850 - protocols used in the energy automation - and some answers suggested using systems from competitors, which doesn't make sense on a forum that is from Siemens. My idea is not to have a Sicam section here, but to give some information and send the colleagues to the right place in order to get more info about Sicam. Mike |
Energy Automation products: Sicam, Siprotec, Digsi |
|
5/20/2012 4:18 AM | |
Joined: 11/18/2009 Last visit: 6/4/2024 Posts: 262 Rating: (18) |
Did you get any answer? |
Follow us on