Industry Online Support
Technical Forum
3/30/2007 7:00 PM | |
Posts: 7 Rating:
|
We are working with S/-PLCSIM V5.3 +SP1 on a PC with XP Pro +SP2 We have to simulate a 5mb program that ,in a productive system, is loaded in a CPU 417-4 The PLCSIM is not able to restart the hardware after downloading Net-Pro. After downloading the Hardware and the complete program, the PLCSIM starts up and after several seconds it is positioned in STOP arguing that it has not enough process time. What can we do? I have attached a zip file with a pair of screenshots and some files with diagnose during downloading netpro, hardware and program. Thanks in advance Attachmentplcsim_cpu417_4.zip (650 Downloads) |
Follow us on