6/13/2012 12:26 PM | |
Joined: 6/13/2012 Last visit: 3/28/2024 Posts: 64 Rating: (0) |
Hi! I have problem while activating my wincc project . The activation stops during the activation of allarm login and runtime doesn't run. I activated graphics runtime,global script, alarm login, tag login and archive user. The version of wincc is 7.0 sp2 Update 1. No antivirus or other programs are installed on the pc, i installed only wincc. My hardware pc is: Model: Acer Aspire M1930 Rating: 220-240Vac, 3.15A, 50Hz Windows 7 Pro SP1 32 Bit CPU: Intel Core i3 Processor 2120 RAM: 4GB DDR3 memory HDD: 400 GB Hard Drive wdc wd5000aakx-001ca0 ata device OPTICAL: PIONEER DVD-RW DVR-219RS ATA DEVICE VIDEO: Nvidia GeForce 510 1024 M LAN: Integrated LAN 10/100/1000 MODEM: none KEYBOARD: USB keyboard MOUSE: USB Optical mouse SPEAKER: None BIOS: P02-A2L I enclose diagnose log file. Thank you Attachmentdiagnose.zip (145 Downloads) |
Last edited by: lakebodom at: 6/13/2012 12:28 PMLast edited by: lakebodom at: 6/13/2012 12:27 PM |
|
6/13/2012 3:23 PM | |
Joined: 12/14/2010 Last visit: 6/28/2023 Posts: 160 Rating: (6) |
Hi lakebodom, look here too: http://boardreader.com/thread/Alarm_Logging_RunTime_does_not_start_6r19zX4210.html You are using programs from third makers for to clean the Windows registry ? best regards. |
6/14/2012 12:28 PM | |
Posts: 1776 Rating: (95)
|
Hi, mave you anywhere a Windows XP? see the downgrade option at Microsoft http://www.microsoft.com/oem/en/licensing/sblicensing/pages/downgrade_rights.aspx |
6/19/2012 9:12 PM | |
Joined: 6/13/2012 Last visit: 3/28/2024 Posts: 64 Rating: (0) |
Thank you very much!!! |
This contribution was helpful to1 thankful Users |
Follow us on