6/26/2012 1:02 PM | |
Posts: 88 Rating: (1) |
Dear all, I have an odd question. i want to install wincc runtime on wincc server computer, I've installed as I knew and loaded the project from engineering computer to the server. on sever computer i set the project to come up at start up via AUTOSTART menu, but this not happen,besides i expect to see the wincc runtime icon on my desktop but i don't. any help in appreciated in advance AttachmentFull page fax print.pdf (211 Downloads) |
6/26/2012 2:08 PM | |
Joined: 10/3/2010 Last visit: 9/27/2024 Posts: 1562 Rating: (191) |
Did you open the project on the server first manually to change the computer name? |
B r g d s , |
|
6/27/2012 7:16 AM | |
Joined: 10/3/2010 Last visit: 9/27/2024 Posts: 1562 Rating: (191) |
Weird, did you install as administrator? |
B r g d s , |
|
6/27/2012 7:30 AM | |
Posts: 88 Rating: (1) |
Sorry what do you mean exactly? I've installed wincc run time on the server computer with the administrator user loged in |
6/27/2012 7:33 AM | |
Posts: 88 Rating: (1) |
i've attached the installation path of wincc runtime on the wincc server computer, I guess there is somthing wrong with the installation :( best regards |
6/27/2012 1:16 PM | |
Posts: 88 Rating: (1) |
Solved, it was the problem of station configurator. Best Regards |
This contribution was helpful to1 thankful Users |
Follow us on