6/27/2012 11:23 AM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating:
|
I am using CPU414-H SYSTEM, AND I HOPE THERE WILL BE AN FAQ SIMILAR TO YOU POSTED FOR CPU-414 ALSO. LET ME FIND OUT. ADDITION, YES THERE IS AN MMC
|
Last edited by: Lucky123 at: 6/27/2012 11:23 AM |
|
6/27/2012 12:54 PM | |
Joined: 10/7/2005 Last visit: 9/12/2024 Posts: 3020 Rating:
|
Hello nbk could it be that you are "missing" to look at the exponent of the Real number |
Cheers |
|
This contribution was helpful to
2 thankful Users |
6/27/2012 11:25 PM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating:
|
Nbk, Please take a look at the attachment, and see IN3, you may see the value 1.200e+003, which means it is a real number and indeed is 1200.0 e+000=1.2 e+001=12.0 e+002=120.0 and so on. I hope it make sense to you now.
AttachmentNk_see.pdf (298 Downloads) |
This contribution was helpful to
2 thankful Users |
6/28/2012 6:31 PM | |
Posts: 197 Rating:
|
@ Lucky123. "e+001=12.0" Indeed, my counts in DB3.DBD0 were 1.000000e+001, 1.100000e+001, 1.200000e+001 for its integer equivalents of 10,11, 12 and so on !! .............. which means the codes were doing good ; I wasn't "seeing" good !! ........ Actually, this was the first time I ventured into number conversion codes purely driven in by the interesting post of Lucky123. Thanks dear fritz/ Lucky123. (The attachment is a bit distorted ........ but I got your point) Regards |
This contribution was helpful to
2 thankful Users |
Follow us on