Industry Online Support
Technical Forum
6/29/2012 10:21 PM | |
Posts: 74 Rating: (3)
|
Hello Davinder. Your local Siemens office is a good place to start. We have PI people in Dubai office that know the product. The truth be known, ultrasonics works pretty well on diesel because it has pretty constant vapour and is not so volatile. So, you could use a ProbeLU or a Multi 100/200. The ProbeLU can be ordered with Profibus PA and would be the most cost effective. My first choice for your application, though, would be a high frequency radar sich as the LR250. The LR200 or ProbeLR is low frequency (6GHz) and it should not be used with low dK liquids since it penetrates into the liquid. The LR250 (26GHz) can be mounted from the top and does not require a stilling well, in fact it will work better without one. If the application is less than 10 m, please check out the LR250PVDF. It can also be ordered with Profibus and would provide the best accuracy. Ref site: https://www.automation.siemens.com/w1/automation-technology-sitrans-lr250-pvdf-24602.htm Regards Toppie [ |:) |
This contribution was helpful to2 thankful Users |
Follow us on