7/1/2012 8:56 AM | |
Posts: 14 Rating: (0) |
Need Of GSD file for (Siemens Simatic S7 6ES7-374-2XH01-0AA0 I/O Module) .... |
7/1/2012 9:41 AM | |
Joined: 10/7/2005 Last visit: 11/11/2024 Posts: 3026 Rating: (1057) |
Hello msarapong the 6ES7374-2XH01-0AA0 is a Simulator module and you will NOT find a GSD file it as it isnot a Profibus DP Slave by itself, but simply a Signal module for an S7-300 and/or ET200M Profibus DP Slave station. Have a look at the Hardware update for 6ES7374-2XH01-0AA0 simulator module thread to find out how to configure and use it, should that be the information you are actually after. I hope this helps P.S: It would be greatly appreciated if you only post a question once in the future (posting the same question three times in three different conferences does not increase your chances of a receiving a useful answer). |
Last edited by: fritz at: 7/1/2012 9:42 AMtypos Cheers |
|
This contribution was helpful to1 thankful Users |
7/1/2012 2:31 PM | |
Posts: 14 Rating: (0) |
Thanks for your suggestion. It is working |
7/2/2012 8:51 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread Need Of GSD file for Siemens Simatic S7 6ES7-374-2XH01-0AA0 I/O Module Best regards O_Moderator |
Follow us on