Industry Online Support
Technical Forum
4/10/2007 11:45 AM | |
Posts: 25 Rating: (3) |
Dear all, This is a Protool project for Op7 which is migrated to OP77B and then the device type is changed to OP77A since the direct migration tool is unavailable. Im facing problem with the "Errors and Warnings" of the WinCC flexible 2005 adv SP1 for OP77A panel. The Warning Messages which are called Event messages in Protool are not getting Displayed in the HMI. I have added a template page and pasted an Alarm window.I have enabled theDisplay properties for Warnings and errors. I have also tried creating my own Alarm class and enabling in the display properties.But still it is not working. If i declare as errors, Thenit is getting displayed but every time the OPeratorhasto ACK it with ACK button.The customer doesnot want that.What is the solution?? I have attached the pdb file and the screen shots. AttachmentOP77A_Screens_PDBFile.zip (140 Downloads) |
Follow us on