7/19/2012 1:26 PM | |
Posts: 1530 Rating: (59)
|
Hallo roohallah, have you already seen this FAQ: How can you create a Windows MessageBox and have the button pressed by an operator evaluated? Did you already take a look at WinCC Information System and type in "MSGBox Function". There you will get more detailed information about possibilities you have. Could you please tell me where you want to make a convertation? Best regards Bizur |
7/23/2012 9:57 AM | |
Posts: 139 Rating: (0) |
hi bizur thanks for your answer example: int a=5; MessageBox(NULL,NULL,a,MB_OK); ERROR: type mismatch in argument 3 |
7/24/2012 12:11 PM | |
Joined: 3/15/2010 Last visit: 6/18/2024 Posts: 137 Rating: (9) |
The arguments in MessageBox function must be strings (check here for futher information on usage). Here is one example of application: [code] int a; int answer; char text[255]; a = 5; sprintf(text, "Change value to %d?", a); answer = MessageBox(NULL, text,"Warning!",MB_ICONWARNING|MB_SETFOREGROUND|MB_SYSTEMMODAL|MB_YESNO); [/code] This will trigger a Message box with Yes/No buttons, with the specified text. Good luck! |
8/10/2012 9:02 AM | |
Posts: 139 Rating: (0) |
HI MY FRIENDS I GET ITS SOLUTION: USING strcmp FUNCTION |
This contribution was helpful to1 thankful Users |
Follow us on