8/16/2012 4:22 PM | |
Posts: 8 Rating: (0) |
GREAT! Thanks for Your answer. This means I can control this big (8 meters) three axis saw for granite using encoders with Logo! Thanks again! |
8/16/2012 8:49 PM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
Note that de Low Voltage LOGO! serie 0BA6 has 4 high speed inputs. Ist enough for counting 3 axis. |
8/17/2012 1:06 PM | |
Posts: 8 Rating: (0) |
I'm using 0BA7 24V and it also has 4 fast inputs. I'm using three of them, one for every axis. |
8/27/2012 8:44 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi MaciejP, please remember the following facts about the high speed puls inputs: a) The "cnt" pin of the (or a) counter must be direct connected with an input pin - If not, then the maximum rate is only 0.5 * fz (with fz = LOGO! cyclic frequency) That means, that the using of high speed input pulses is verry difficult and for the most applications not good usable - because the LOGO!-cycle frequency is to low, sorry! Best regards |
==> Meine TAG-Listen: "deut." |
|
Follow us on