10/2/2012 7:19 AM | |
Posts: 5 Rating: (0) |
I use PCS7 7.1 sp1with APL 7.1. When I click the APL icon, WINCC RT can't open the APL Faceplate and have "SCRIPT :OS0X02 Action Error" Error Message NO is1007001. I find the description of the alarm is "If it concerns a Global Script action, the connection to the action name can be made via the application window GSC Runtime, as long as the runtime has not been restarted or a Global Script action is saved." Attachmentapdianose.pdf (105 Downloads) |
Follow us on