Industry Online Support
Technical Forum
11/14/2012 10:12 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665) |
Hello Pourya; The only way to implement a SIL 3 level program with a S7-300 is to use a F-CPU (such as the S7-317F-2DP), F-IOs and the programmingpackage Distributed Safety (along with Step 7). And yes, downloads of the safety program to the PLCwill require you to go to STOP mode (or the CPU will shut down when you attempt it). See the following thread, you will find excellent advice and good links from members yy1 and fritz to pursue your search: Safety Program modification & Compile & Download. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/14/2012 10:14 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on