Industry Online Support
Technical Forum
11/29/2012 1:17 PM | |
Posts: 1547 Rating: (129)
|
Hello, yes it is possible and it works fine. Controler and Device at the same time could be the following CPs: CP 343-1EX30 CP 343-1GX30/31 For this kind of application you have to use special function blocks. Please have a look under the following link: How do you program communication blocks FC11 and FC12 for the PROFINET IO controller? http://support.automation.siemens.com/WW/view/en/26558253 How do you program communication blocks FC11 and FC12 for the PROFINET IO device? http://support.automation.siemens.com/WW/view/en/31764615 |
Follow us on