(0)| 10/24/2005 11:33 PM | |
|
Joined: 8/25/2005 Last visit: 1/14/2026 Posts: 1162 Rating:
|
Hello Darius, the GSD files you find here should be the newest which exist. PROFIBUS GSD files : SIMATIC Which DP-Master you are using? If it is an S7-Station: The best way to configure the hardware is to include the DP-Slave as an existing station. Please give us more informations about the error message you get. Maybe you have configured an older CP? Or the modules arn't exactly the same? If it is possible for you, post the information of the diagnostic puffer. Maybe as an attachment? Best regards Sabine |
Last edited by: Hulzhex at: 10/24/2005 11:33 PM |
|
Follow us on