Industry Online Support
Technical Forum
12/19/2012 9:50 AM | |
Posts: 12 Rating: (1) |
Hello; In my project hardware configurastion is; CPU 313C (6ES7 313 1BG04 0AB0) + CP343-1 (6GK7 343 1 EX30 0XE0) 1. zone =ET200S (6ES7 151 3AA23 0AB0)+ PM +8DI DC24V ST(x 2) 2. zone =ET200S (6ES7 151 3AA23 0AB0)+ PM +8DI DC24V ST(x 2) 3. zone =ET200S (6ES7 151 3AA23 0AB0)+ PM +8DI DC24V ST(x 4) 4. zone =ET200S (6ES7 151 3AA23 0AB0)+ PM +8DI DC24V ST(x 3) 5. zone =ET200S (6ES7 151 3AA23 0AB0)+ PM +8DI DC24V ST(x 2) In OB1 calling FC12 to receive inputs from ET200S over CP343-1 it is good working until LEN = 8 but LEN= 9 and over FC12 ERROR = 1 I could not understand what is the problem? is the max length = 8 byte in this configuration or whatis thewrong thing. In the attachmet you can see the configuration for1. zone and just 8DI, it is working My new confguration is like above. I need you comment. Thank. Erol Attachmentconfig.pdf (60 Downloads) |
Follow us on