Industry Online Support
Technical Forum
1/18/2013 10:23 PM | |
Joined: 3/14/2008 Last visit: 9/26/2024 Posts: 2098 Rating: (938) |
It should be in the PCS7 catalog...this means that the module is supported... You can check by selecting the standard step 7catalog in the upper right corner instead of the pcs7 catalog. It lists all siemens hardware |
If I could help you, you can use the RATE button. Thank you. |
|
1/21/2013 11:31 AM | |
Posts: 836 Rating: (100)
|
Hi, the 41x-5H CPUs are supposed to be used with PCS 7 V8.0 Update 1 (check out this entry). Since PCS 7 V7.1 SP4 you should be able to use 41x-5H but only for spare part compatible use. Check out this entry for further infomations. Ithink that you won't be able to download your HW config to the 417-5H with PCS 7 V7.1 SP3. So either you update to 7.1 SP4 or you use PCS 7 V8.0 Update 1. Where did you get the information that you can use 41x-5H with PCS 7 V7.1 SP3? |
Last edited by: Silent Bob at: 1/21/2013 11:33 AM |
|
Follow us on