Industry Online Support
Technical Forum
1/28/2013 6:45 PM | |
Joined: 5/6/2012 Last visit: 10/17/2024 Posts: 13 Rating: (2) |
I have some projects with step 7 , where I configured. OPC is used for diagnostics with SNMP . In the configuration I defined PC station with OPC + IE + General Winccflex In the properties of OPC + SNMP , Edit plant configuration , I configured the nodes where should I make the diagnosis . Now I use TIA Portal, where I set up the equivalent of properties of OPC + SNMP , Edit plant configuration ? Step 7 v5.5 +sp2+hf4 WinccFlex 2008+sp3+up3 Simatic net v8.1+sp1 Tia_Portal V11+sp2+up5 Thanks AttachmentD:\case\OPCSnmp\OPC_SNMP.zip (250 Downloads) |
Follow us on