Industry Online Support
Technical Forum
1/18/2013 6:12 AM | |
Posts: 2 Rating:
|
When u go to constant power mode above basic rated frequency the freq can be set to 60 / 63 hz to achieve 3600 RPM but torque falles inversely |
2/7/2013 8:08 AM | |
Posts: 129 Rating:
|
how much percentage of speed can increase compare to motor rated speed???? |
2/7/2013 8:10 AM | |
Posts: 129 Rating:
|
what is the difference between V/F, SLVC, TORQUE CONTROL modes with give one example????? |
2/7/2013 9:29 AM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating:
|
Hello, see capture 4: http://support.automation.siemens.com/WW/view/de/59737625/0/en general: V/f: for example for pumps and fans Vector control (with or without encoder (SLVC)): If you need a high speed accuracy (with encoder its better - especially for low speeds). Torque control (for example winders which work tension controlled). Zako |
Follow us on