Industry Online Support
Technical Forum
2/7/2013 6:06 PM | |
Posts: 1547 Rating: (129)
|
Hi, Using 5GH and the right antennas up to 10km are possible - given you got aclear line of sight between them. The 1000m you found maybe were about 2,4GH? There's a good tool for choosing components available here: www.siemens.de/snst > Just to get an idea whether a setup can work or not. Attached some "random" choice that should do the trick. Better yet ask the presales support about details. If there is no line of sight in between, maybe VPN withScalance S612 plus MD741 / M875 (GRPS/UMTS) is an alternative for some stations. |
This contribution was helpful to3 thankful Users |
Follow us on