Industry Online Support
Technical Forum
3/11/2013 9:17 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, 1. The PC in which is installed Step 7 must be connected with CPU and in PG/PC Interface to be assigned the way. 2. Upload Station to PG - Upload the content of PLC to Simatic Manager with no comments and symbols. In order to do corresponding CPU must be assigned during Upload procedure. 3. Download - From Step7 to PLC. Downloading a project (or blocks only) to a selected CPU. There is a manual -SIMATIC Programming with STEP 7 V5.5 Best regards, Hristo Mihalev
|
This contribution was helpful to1 thankful Users |
Follow us on