3/12/2013 2:48 PM | |
Posts: 13 Rating: (0) |
How do I get WinCC RT to "see" that there is a valid license on the computer? We had a 2048 tag license but found that there is >2200 tags. I obtained the upgrade license (2048 > 8192) and tranfered the license over to the C drive. When I checked it the 2048 is now gone and 8192 shows up as an "upgrade" See attached pdf of the screen snap shots. Page 1 - Error message that keeps on coming up but program still works and you have to keep acknowledging the error window Page 2 - License keys on the PC showing license but "unknow" status shown Page 3 - Once status symbol is right clicked and checked its shown as OK but not in use but the program is running. Running on what??? Any assistance to cure this annoyance would be greatly appreciated. System is on a ship so access is not always easily available. Also what is meant by: License types (single, floating and upgrade)? Regards, Barry AttachmentWinCC License Issue.pdf (141 Downloads) |
3/12/2013 3:29 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello Barry, Page 1 : Can you Please Checked the Detail Button on that to Find out Which License is Missing ? Page 2 : Select All License Key & Checked, What it Showing, For Upgrade License You need old 2024 Tag License on Same Drive, Then you can able to Upgrade it, When you Follow the Step Below then You will See the 8K License as a Floating. If you have to upgrade a licensce key in order to use a new software version, please note that you must store the "old" license key along with the upgrade itself on the hard disk of the PC, where the upgrade is to be performed. To upgrade a license key please proceed as follows:
Have a Look on this FAQ Then You will Not Receive the Message Again. |
Last edited by: Ammy at: 3/12/2013 3:33 PMChange the Link Ammy |
|
3/12/2013 6:56 PM | |
Posts: 13 Rating: (0) |
Thanks, they say this seemed to work as the 8192 now shows in use. The 2048 disappears though as I guess it would after the upgrade took place |
Follow us on