3/13/2013 7:17 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello jkt_2 are you using the Flow Meter for the Water Line ? if yes then Have a look on the following Link How to Calculate the Flow using Totalizer..... |
Ammy |
|
3/13/2013 8:21 AM | |
Joined: 10/23/2012 Last visit: 9/24/2024 Posts: 39 Rating: (0) |
hello Ammy my water meter showing the odometer readings so how can i read the odometer readings to plc
|
3/13/2013 9:27 AM | |
Joined: 1/21/2013 Last visit: 10/8/2024 Posts: 4620 Rating: (708) |
Hello jkt_2, You should give us some more information, type of meter, communication protocol, etc.. |
3/15/2013 5:34 AM | |
Joined: 10/23/2012 Last visit: 9/24/2024 Posts: 39 Rating: (0) |
i am going to use water meters with modbus communication then how.. |
3/15/2013 2:45 PM | |
Joined: 1/21/2013 Last visit: 10/8/2024 Posts: 4620 Rating: (708) |
Hello jkt_2, Ammy are right, follow what it says, maybe this can help you. Have a look: Modbus Sample Project Hope this help |
Follow us on