Industry Online Support
Technical Forum
6/5/2007 8:29 PM | |
Posts: 8 Rating: (0) |
Hi, kindly find the attachment. In place of S7y I have TP 177A, fresh from the manufacturer and never been configured. Item 4, is also a bus connector with PG port. My laptop have a RS 232 port only, which is communicating well with the S7x (S7 CPU 314 in my case).In place of profibus cable I am using 2 wire of a 6 core screen cable. Under this connection, when I am clicking accessible nodes from Simatic manager, I can see my CPU node only and not the TP. WhenI am trying to download my WinnCC flexible project, I can't and giving an error message...check settings, ports, cable, etc... Please help regards, Attachmentmpi problem.zip (103 Downloads) |
6/6/2007 8:42 AM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
closed cause question posted twice. Here you will find the second topic: Problem downloading to TP177A - fia MPI adapterin the same conference Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on