Industry Online Support
Technical Forum
5/16/2012 9:24 AM | |
Posts: 3 Rating: (0) |
I have configured a total of 6 Hischmann Switches (Four MS20-0800 & Two MS20-1600) as Profinet I/O using the Hirschmann GSD files to communicate back to S7-300 plcs. The problem I have is that I was expecting Input/Output address for the switch status from the GSD configuration file. However, I'm only getting Diagnostic data address. Moreover, I have configured the SFC 51 to capture the Profinet I/O Diagnostic Address from the unit but receive HEX data, which does not seem to correlate with the Hirschmann switch I/O status mapping table. It's my believe the GSD files have the Input/Output address turned off. Questions: 1) Does anyone have an example project to get status data out of the Hirschmann switch from the Diagnotic Address once configured for to be on Profinet? 2) Does anyone have an example project to get status data out of the Hircschmann switch from the I/O data Address of an updated GSD file with I/O status enabled? Any help would greatly be appreciated. Also, the solution has to come from the PLC not an extra software that can do this automatically (i.e. Industrial HiVision). Much Appreciated, famador1234 AttachmentUM_IndustProtocol_Rel70a_en.pdf (220 Downloads) |
Last edited by: famador1234 at: 5/16/2012 9:28 AMMS20 correction Last edited by: famador1234 at: 5/16/2012 9:26 AM |
|
5/16/2012 12:56 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Just a question not a solution. Have you made the GSD yourself or you are using downloaded Hirschmann GSD?
|
5/15/2013 12:09 PM | |
Posts: 19 Rating: (0) |
Dear friend Really appreciate for the data you have been shared regards soroosh shalileh
|
Follow us on