5/22/2013 10:21 PM | |
Posts: 9 Rating: (0) |
gud day! can anybody tell the difference of cpu 224 (1bd22 ) and 224 (1bd23). b-coz when i transfer the program to cpu 224(1bd23) .the program does not work when i started it.i check the program that i uploaded to the old cpu and the one that i downloaded its perfectly the same. iam using microwin sp6.
AttachmentUnfiled Notes.zip (69 Downloads) |
5/23/2013 8:00 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello. The 1BD23 is the direct succesor of the 1BD22 and should work. Attached you find dasta of both CPU to compare. I would upgrade Microwin to SP 8 orSP 9: STEP7 MicroWIN V4.0 SP8 and SP9 After that try again. Is the whole program not running or are there problems with specific functions? Regards, Marcjan Attachmentcpu224.pdf (81 Downloads) |
Problem solved? |
|
Follow us on