5/27/2013 6:17 PM | |||||||||||||||||||||||||||||||||||||||||||||
Posts: 767 Rating: (69) |
Hello Dan, Unfortunately, from reported data you will not be able to operate this Mitsubkshi motor with SINAMICS S110 drive because the motor is being reported as 1 Phase 230 Volt. Even though the SINAMICS S110 drive can have an input supply of 1 Phase 230 Volt AC, its takes the input power, creates an internal dc bus voltage of approximately 300 Volts DC, then crates an output of 3 Phase 230 Volts to motor. I recommend you consider such as motor as the following SIMOTICS 1FK7 servo motor: Note 1: Make sure your drive has at least as much rated current as the static current rating (i.e. current 100% of time near zero speed)of the motor chosen. Note 2: If you select a motor with an absolute value encoder then user of machine will not need to home machine to a sensor after power is removed to machine. 1FK7022-5AK21-1VH2 Static Current 1.8 Amps Rated Power 0.38 kW Rated Torque 0.6 Nm Holding Brake Rated Speed 6000 rpm IP65 Mitsubishi motor partial data from internet: Rated Power 0.100 kW Holding Brake Rated Torque (calculated) 0.32 Nm Rated Speed 3000 rpm IP65
The following website [CAD CREATOR] is available from internet for additional drawings, technical data, etc. Best Regards, Deputy |
||||||||||||||||||||||||||||||||||||||||||||
5/27/2013 7:30 PM | |
Posts: 767 Rating: (69) |
Hello Dan, Following is the link to the CAD Creator website: http://staging04.it-motive.de/CADCreator/VorNavigation.cfm?IdListVornavi=(0-1*906)&CFID=3430537&CFTOKEN=83380690&Scenario= Alternatively, you may use a search engine such as Google, enter CAD Creator and the link will be in first few hits. If you know part number of interest type part number in upper right corner of screen. Else, select motor type by interest of first four digits of part number. Example: - Click on SIMOTICS 1FK7 - Click on Order Number - Interactively build complete part number one digit at a time - Once part number is complete you may view preview drawing in pdf format -If desire AUTOCAD drawings(2D) or many different types of 3D drawings these are available within seconds by entering email address. Best Regards, Deputy |
Follow us on