Industry Online Support
Technical Forum
5/30/2013 7:11 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
Hello, Have you checked the following topics: DP link between CPU 315-2DP (slave) and S7-400 (master) with STEP 7 V5.3 Configuring Master/Slave 313c 2DP2plc via profibusBest regards Hamid Hosseini |
6/5/2013 7:17 PM | |
Posts: 16 Rating: (0) |
into which plc i need to download the configuration ; s7 400 to PC via MPI or should i configure it individually and download . |
Follow us on