6/7/2013 8:21 AM | |
Joined: 2/20/2012 Last visit: 4/23/2018 Posts: 11 Rating:
|
Hi kcwoodw2, the tool you mentioned from Microsoft ist not released and tested with PCS 7. You can either have a look at the PCS 7 compatibility tool or the software compatibility lists, you find both in the following link: http://support.automation.siemens.com/WW/view/en/2334224. But there is a tool called "SIMATIC Management Console" which is released for PCS 7 since V8.0 SP1: http://support.automation.siemens.com/WW/view/en/72882729. This is intended for the use you described and also has some additional features. I think this can be the solution for you! |
Gruß / Regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on