6/15/2013 11:10 AM | |
Posts: 16 Rating: (0) |
Dear Sir, Iam using 313C-2DP as a DP master with ET200S IO's, now can i connect wincc scada PC on MPI. |
6/15/2013 11:20 AM | |
Posts: 16 Rating: (0) |
I need help soon plzzz reply |
6/15/2013 11:35 AM | |
Posts: 16 Rating: (0) |
Dear Marcjan, Iam using 313C-2DP as a DP master with ET200S IO's, now can i make MPI as a DP slave |
6/15/2013 2:03 PM | |
Joined: 9/27/2006 Last visit: 5/27/2024 Posts: 12257 Rating: (2668)
|
Hello manohan; For all WinCC communication issues, please have a look at the following manual : WinCC: Communication If you have a different version of WinCC, look for the specific communication manual for that versionon the forum Support Pages, using the search box at the right. But you will find that as far as interfaces are required the information does not change very much between versions. MPI, Profibus and various other protocols for S7 PLCs are handled in WinCC as part of a S7 Protocol Suite channel. The interfaces required for establishing the comm link between the WinCC PC and the PLC are described briefly in the attached document. For more information, try the WinCC Online help or read further in the suggested manual. Hope this helps, Daniel Chartier |
Follow us on