Industry Online Support
Technical Forum
6/26/2013 5:08 PM | |
Posts: 767 Rating:
|
Hello bright, Depending upon such items as motor type, feedback type (if applicable), hardware interface, and possible control interface most likely the Simodrive 611universal would be recommended replacement. Following is a link to information for Simodrive 611universal. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid0=10804940&objid=10804940&onlyConfigurable=on&subtype=130000&lang=en&extranet=standard&viewreg=WW&u=NDAwMDAxNwAA&siteID=cseus Deputy |
6/26/2013 8:41 PM | |
Posts: 2964 Rating:
|
Hello, I think he needs the replacement for 650 Drive.....It will be with Simodrive 611A with 120KW with the Simodrive 611U. Regards, Prakash |
Follow us on