6/30/2013 6:58 PM | |
Joined: 9/17/2007 Last visit: 4/17/2023 Posts: 799 Rating: (82) |
Moin, can you write the application name behind the simatic numbers |
VG / regards vanDyk |
|
6/30/2013 8:15 PM | |
Joined: 9/7/2007 Last visit: 10/9/2024 Posts: 550 Rating: (62) |
HiRaymondk IT is so strange to use WinCC OA for this application. WinCC OA is for extra large projects than WinCC. if you have 3 machines I claim that WinCC will be quite sufficient. You can use more than 150K Power Tag!!!
|
Best Regards |
|
7/3/2013 7:36 AM | |
Posts: 39 Rating: (1) |
please mention the details |
7/3/2013 11:46 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 9/7/2007 Last visit: 10/9/2024 Posts: 550 Rating: (62) |
Hicorleone WinCC OA is an Extra Large SCADA system introduced by Siemens to cover projects larger than what is covered by SCADA WinCC. WinCC OA formally was named PVSS (a product of an Austrian company named ETM ) that Siemens brought to cover this market sector. Here is the system technical Specifications
1) Dependent on the available storage space 2) Dependent on the system configuration and the system load (due to the event-oriented architecture, the system load is essentially determined by the change rates of the values to be processed) 3) By means of high-performance hardware configuration (one archiving cluster and approx. 120 distributed systems that archive parallel values in the cluster): 200,000 archived value changes per second 4) Physical limit: <2048, in practice systems have already been implemented with up to 550 distributed systems 5) Physical limit: < 244 clients per server, recommended: max. 100 clients per server For More information: |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Best Regards |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
7/7/2013 4:27 PM | |
Joined: 9/7/2007 Last visit: 10/9/2024 Posts: 550 Rating: (62) |
DearRaymondk Although you have a small number of process tags, but you want archive and historical data for trends and alarms. WinCC will fill your requirements. |
Best Regards |
|
Follow us on