7/9/2013 9:12 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
May be this is what you are looking for http://www.energy.siemens.com/us/en/automation/power-transmission-distribution/protection/siprotec/multifunction-generator-motor-and-transformer-protection-relay.htm Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
7/9/2013 3:07 PM | |
Joined: 10/9/2007 Last visit: 5/21/2024 Posts: 1241 Rating: (115)
|
Hi I'm not sure you will find today a device which does only one single protection fuction.Maybe for someespecific protection fuctions. From the Siprotec line you could use the 7SJ46, which is a compact device programmed by DIP switches and only has overcurrent protection http://www.energy.siemens.com/ecc_pool/SIPROTEC4/860467a1-e231-4b11-b202-781fae87119e/7SJ46_Catalog_SIP_E6.pdf Or 7SJ600, which is a compact device with not so many protection functions, but more than 7SJ45 and configurable via Digsi: http://www.energy.siemens.com/hq/en/automation/power-transmission-distribution/protection/siprotec/?dlsearch=1&fiProductFamily=SIPROTEC 4&fiProductName=7SJ600 This device is used for small motor, feeder protection andas backup protection, like earth fault protection on trafos. Mike |
Energy Automation products: Sicam, Siprotec, Digsi |
|
Follow us on